Description
Reads the state of one digital input according to the number identified in the command.
Examples
Code
--> DIN1.STATE 1
Context
See Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
|
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
20000 |
1 |
20000 (0x4e20) |
DIN1.STATE |
Unsigned8 |
Read Only |
Yes |
|
20001 |
1 |
20001 (0x4e21) |
DIN2.STATE |
Unsigned8 |
Read Only |
Yes |
|
20002 |
1 |
20002 (0x4e22) |
DIN3.STATE |
Unsigned8 |
Read Only |
Yes |
|
20003 |
1 |
20003 (0x4e23) |
DIN4.STATE |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DIN1.STATE |
20000 |
Unsigned8 |
Read Only |
- |
|
DIN2.STATE |
20001 |
Unsigned8 |
Read Only |
- |
|
DIN3.STATE |
20002 |
Unsigned8 |
Read Only |
- |
|
DIN4.STATE |
20003 |
Unsigned8 |
Read Only |
- |